New M12 Y distributor with assembled cable

The new M12 Y distributors with a connected cable provide more flexibility in the sensor/actuator cabling and enable new approaches for machine and system cabling.


Using these, two adjacent sensors with only one cable can be easily and cost-effectively led to the next sensor/actuator box or control system.

This eliminates the second sensor/actuator cable and simplifies the installation. The new Y distributors with their two slots are thus virtually the smallest sensor/actuator boxes available in the market.

M12 Y distributor at open conductor end
M12 Y distributor at open conductor end




M12 Y distributor on M12 connector
M12 Y distributor on M12 connector
The distributors have the IP67 degree of protection and are available in versions with different cable lengths with open cable ends or with assembled M12 connectors with SPEEDCON quick locking.

It is possible to have other versions even in a shielded design on request.




Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00