M12 flush-type connectors with plastic housings

In the industrial area, there are always applications where field devices and their connections come into contact with aggressive substances.


These substances can cause corrosion on the connector housings.As an alternative to the familiar stainless steel variants, which are often used under such ambient conditions, there are now flush-type connectors available with plastic housings.

The plugs and sockets are made of polyamide and are available in 5- and 8-position versions.The plastic variants are available with punched on individual wires, solder cups or solder pins for PCB mounting.

M12 flush-type connectors with plastic housings
M12 flush-type connectors with plastic housings



Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00