With touch panels more automation at a glance
The TP 06T, TP 10T, TP 12T, TP 15T touch panels are powerful devices with which big machines or even entire production systems can be operated and monitored.
They have an industrial, resistive touch display that is embedded in a noble and solid aluminum front. The touch panels are now available with double processor power.
Simple visualization
Significant function expansions have been made using the Visu+ 2.0 version. A particular highlight is that these touch panels can be operated on a Siemens S7 controller via Ethernet TCP/IP.
For customers who want to remain with Visu+ 1.2, Phoenix Contact offers corresponding FW versions on the Internet. We thus facilitate a smooth transmission to the new versions without project and time pressure.