Service Pack 1 for the AUTOMATIONWORX Software Suite 1.50
Service Pack 1 for the AUTOMATIONWORX Software Suite 1.50 is now available for downloading. The following new functions are supported:
- PC Worx 6.0 now supports numerous additional controllers / firmware states from the Inline Controllers up to S-MAX
- Startup parameterization for various PCP devices
- Entering virtual IP addresses
- Import / export interfaces for networks / bus systems
- Expanded settings for GSM/GPRS
- Collectively used function blocks and data types

Download Change Notes
Debugging has also taken place. All changes have been listed in the Change Notes in the Download Center under the following link: