Signal acquisition in extremely harsh ambient conditions
Whenever maximum durability and fast replaceability are required, Rugged Line devices from Phoenix Contact are the perfect choice. These devices can now also be used in Profinet networks.
The new digital input and output module has been designed for use in system engineering and can for example be used on tool platforms, directly on welding robots or in conveyor systems.
The new Rugged Line Profinet IO devices from Phoenix Contact

Use in the automotive industry
Ideal for the harsh ambient conditions in the automotive industry
Thanks to the use of VARIOSUB Push-Pull connectors for network and supply voltage, this device is also suitable for use in the automotive industry.
The first device in the range has eight fixed digital inputs and eight freely configurable inputs and outputs each with a current carrying capacity of 500 mA. More variants are presently in the planning stage.