Service Pack 2 for AUTOMATIONWORX Software Suite 1.40

 Service Pack 2 for AUTOMATIONWORX Software Suite 1.40 is now available for downloading. The following new functions are supported:

  • PC WORX now supports the RFC 470 PN 3TX,
    ILC 170 ETH 2TX and ILC 330 PN control systems,
  • Support of PROFINET/PROFIBUS Proxy FL NP PND-4TX PB,
  • PC WORX EXPRESS is also available in Spanish, French and Chinese (simplified),
  • Support of INTERBUS diagnostics,
  • All diagnostics messages of SAFETY SLC 400 PND-4TX-IB have been revised. Additional information is now provided with the error location with certain messages,
  • The AX OPC SERVER now supports RFC 470 PN 3TX as well.


Download Change Notes


Debugging has also taken place. All changes have been listed in the Change Notes in the Download Center on our homepage with the keyword "Suite" and under the following link:



Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00