Easy planning of wireless systems in industrial environments

There are a few questions that pop up when introducing a wireless system:

  • How does one introduce a wireless system?
  • How should the wireless devices be positioned in the industrial hall, for example?
  • How many devices are required for complete and safe wireless coverage?

The wireless simulation tool provides quick help in answering these questions without taking a lot of processing time. A range of functions enables the simulation of wireless coverage in advance, taking into account various points of view.

Easy wireless system planning through simulation

Easy wireless system planning through simulation

Determine the required quantity and the optimum position for the wireless modules in the infrastructure on the basis of a building plan and by entering a minimum of data. All steps are easily carried out with little instruction, even for system planners unfamiliar with wireless technology.


Brief description of application

  • Integration of a building plan on the basis of graphic formats
  • Calibration of plan to scale
  • Drawing in the building structure on the basis of pre-defined walls from a library
  • Drawing in space fillers such as steel cabinets or machines
  • Selection of wireless components from a list and positioning via a mouse click
  • Simulation in various views and display types
  • Adaptation of transmission power or antennas for special applications
  • Easy optimization of wireless coverage on graphical interface
  • Determination of the required wireless components, printing the result as a graphic


Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00