Safe use of Ethernet installations

The security of Ethernet networks in companies continuously receives greater importance. Independent studies show that more than 70% of network errors and crashes are due to faulty cabling infrastructure and manipulation on the connection cables.

By using factory line patch cables as well as new accessory products, the security requirements in the automation environment and the control level are completely fulfilled and any potential error sources are already eliminated beforehand and the network availability is increased.

Patch Guard


In connection with the Factory Line patch cables, the FL PATCH GUARD provides the only way to secure ports which cannot accept security frames. In this way, it is possible for the first time to secure ports on any Ethernet components, e.g. controllers.

Thanks to the slender design, it is even possible to connect Patch Guard elements directly to switches with high port densities, such as the FL SWITCH MCS... It is only possible to release connections with a special key.

Patch guard by Phoenix Contact
FL PATCH GUARD - Securing ports on any Ethernet components



Plug Guard


Plug guard by Phoenix Contact
FL PLUG GUARD really makes network connections secure
The concept of FL PLUG GUARD... is specifically suited for Factory Line switches and patch fields with smart holes. Connections can only be severed by authorized personnel with the aid of a key.

Unused ports can also be effectively protected from unauthorized access in conjunction with the Fl Port Guard locking elements.




Safe Clip


The FL PATCH SAFE CLIP securing element can be mounted without tools and prevents Ethernet connections from being disconnected unintentionally. The protected connections can only be disconnected if conscious action is taken.

By means of this simple and quick to install solution, unintentional disconnection is reliably prevented.

Safe Clip by Phoenix Contact
FL PATCH SAFE CLIP - Accidentally releasing Ethernet connections is not possible



Further information and services related to this article