Axioline - Realtime I/O
The fastest I/O system in the world

Axioline from Phoenix Contact is the realtime I/O system which is able to meet all your requirements in terms of the fastest possible response times and efficient production, providing increased precision in measuring technology and a higher level of dynamics in control and regulation technology.

With Axioline, you will benefit from our expertise from the development of CLIPLINE complete, the modern modular terminal block system:

  • Optimum connection method
  • The most efficient marking solutions
  • Sophisticated design

 

Hinweis
Here we would like to present you a video. Adobe Flash Player is required to view this video. You might need to adjust some settings in your browser if you have alreadinstalled Flash Player.y


Axioline for higher cycle rates and increased levels of machine output

With Axioline, you will be able to access key data, anytime and anywhere. For each module, Axioline has a maximum update time of one microsecond.

At an I/O station with 256 I/Os, the update time of the system is less than six microseconds. This means that time observations are no longer required. Axioline's speed is determined by the bus it is connected to, as Axioline is as fast as parallel cabling. 



The PROFINET system from Phoenix Contact
PROFINET from Phoenix Contact
Axioline is optimized in line with PROFINET

Furthermore, Axioline is open to all Ethernet-based communication
protocols and is optimized in line with PROFINET.




Product features and contact details

Would you like further information about the first realtime I/O system in the world?
Then take a look at our portfolio in the E-shop or get in touch with us.


Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00