Space-saving and compact potential distribution with spring-cage hybrid terminal blocks

The new STU 10/ 4X2,5 and STU 35/ 4X10 spring-cage hybrid terminal blocks from Phoenix Contact offer an interesting alternative to parallel potential wiring. These terminal blocks have a screw connection with a wide conductor cross-section for the power supply.

In terms of distribution, this potential is distributed among four spring-cage connections of a small nominal cross-section. 

Two variants are available. In the case of the STU 10/ 4X2,5 (right in picture), a 10 mm² infeed line is split into four 2.5 mm² connections, and in the case of the STU 35/ 4X10 (left), a 35 mm² infeed line is split into four 10 mm² connections.

Due to the compact design, these hybrid terminal blocks are ideal for use in power supply cabinets in installation engineering.

The STU potential distributors naturally use standardized accessories of the CLIPLINE complete system.